Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
What is anti-rotation? If the extension tube is not kept from turning the actuator
will not extend. Usually the mounting restrains the extension tube easily. But in some applications, like connecting to a cable, it is necessary for the actuator that have a built in anti-rotation
feature. The anti-rotation feature keeps the extension tube from rotating on its own.
This video describes the anti-rotation feature and its usefulness.
This video describes the anti-rotation feature and its usefulness.