Skip to content Skip to navigation

Can the amperage number or limit be set for an actuator?

Using the J1939 messages the user can set the number of Amps the actuator is allowed to see before turning off motor current.  This feature is similar to a clutch, but different in the fact the user gets to set the load at which the unit will trip.

back to top