Zum Inhalt springen Zur Navigation springen
Press Release Hero Image

Thomson Industries to showcase innovative portfolio of Electrak® linear actuators

Thomson Industries, Inc., will be attending Agritechnica 2019 – the world’s leading agriculture machinery trade fair alongside Altra Industrial Motion Corp. from 10th – 16th November in Hanover, Germany.

Delegates and visitors attending the tradeshow will gain an exclusive opportunity to see Thomson’s new Electrak® MD linear actuator, alongside a wide range of electromechanical linear actuators and solutions. Thomson’s broad range of linear actuators delivers high power density, high durability and strength with the ability to exert forces up to 22,000 newtons. The portfolio showcase will include the Thomson Electrak MD, Electrak HD, Electrak Throttle, Max Jac, Electrak GX, Electrak 1 and the Warner Linear M Track, B-Track and H-Track actuators.

Eliminating the need for space consuming external equipment and delivering expanded force offerings, Thomson’s new Electrak MD electric linear actuator provides onboard electronics, high environmental resistance, and a compact design with the ability to carry loads up to 2 kN.

Exclusive to the tradeshow, Thomson will also be highlighting their integrated synchronisation options for the Electrak HD and Electrak MD line of actuators providing more control, power and durability. These features will be shown as a live demo on the booth, in addition to “smart” actuator features such as onboard electronics and built-in SAE J1939 Can bus option showcased in the Electrak HD, Electrak MD, and Electrak Throttle.

Thomson representatives will be on hand throughout AGRITECHNICA 2019 in Hall 15, Booth G24 to discuss the diverse portfolio of application solutions provided by its electric linear actuators. For more information, please visit www.thomsonlinear.com.

About Altra Industrial Motion Corp.
Altra Industrial Motion Corp. gathers leading brands that designs motion control and power transmission products, including Thomson Industries, into a united group of technology solutions. As a team, Altra provides design engineers with decades of application engineering expertise to help find the just-right solution across a host of industries.

About Thomson
With more than 70 years of motion control innovation and quality, Thomson is the industry’s premier producer of Linear Ball Bushing ® Bearings and Profile Rail Bearings, 60 Case ® Shafting, ground and rolled Ball Screws, Linear Actuators, Gearheads, Clutches, Brakes, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of mechanical motion control solutions serving global commercial and aerospace & defence markets. Thomson Industries, Inc. has facilities in North America, Europe and Asia with over 2000 distributor locations around the world.

Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1- 540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

With built-in support for onboard electronics and built-in SAE J1939 CAN bus option, ‘smart’ features provide new possibilities for the integration of electromechanical actuators into agricultural, construction and mobile-off- highway applications.

Thomson will be showcasing the new Thomson Electrak® MD linear actuator, alongside a wide range of electromechanical linear actuators and solutions at Agritechnica 2019.

“Smart” actuator features such as onboard electronics and built-in SAE J1939 Can bus option will be showcased in the Electrak HD, Electrak MD, and Electrak Throttle.

Back to press releases
Zum Seitenanfang