Skip to content Skip to navigation

03/12/2019 | Thomson introduces online, interactive, instant quote tool for customized 60 Case® shafting and hardened pins

12.03.2019 - RADFORD, VA – Thomson Industries, Inc., a leading manufacturer of linear motion control solutions, has introduced an online instant quote tool that helps design engineers save time during the selection and purchase process of its customized 60 Case shafting. By providing real-time pricing and instant access to lead times for chosen products, Thomson’s intuitive, self-service tool allows designers to more quickly and easily procure the correct parts for their machines with special machined options.

For example, a user may require a custom coaxial hole, a flat, a journal reduction, or any other customization or combination thereof. With Thomson’s new online tool, users can easily make design changes in real time and quickly customize from different materials, including carbon steel, stainless steel or chrome plated. Thomson’s intuitive interface can also help users assign threads to tapped holes.

Traditionally, this type of on-demand manufacturing has not been available for linear motion,” said Kyle Thompson, Thomson’s Product Innovation Manager. “We have created a tool that allows our customers to upload their 3D part model and instantly access our component’s price and lead time, and the ability to purchase.” The new instant quote tool also allows users to easily change material and quantity requirements with the click of a button.

60-case sizing tool
Thomson’s new online tool allows customers to upload their 3D part model to instantly access a shafting component’s price and lead time, and have the opportunity to purchase.

Thomson is committed and continues to enhance design engineers’ online experience, improving the ease and speed of the purchase process. “With the online tool, customers are able to complete the purchase process in just a few minutes, eliminating any wait time for a quote response,” added Thompson. “Users are able to immediately see how quantity affects pricing and can use this tool to optimize their designs and compare features in real time.

Traditionally, engineers would be required to design a component using 3D modeling software, then create a toleranced 2D print to be manually submitted to Thomson for quoting. This process could take several days. Any changes to the 3D model would need to be reflected in the 2D print and then resubmitted for quoting. With Thomson’s new online instant quote tool, engineers can simply upload their 3D model to see price and lead time and are even provided with the option to order the product immediately. “The tool eliminates the need for a 2D drawing, enabling design engineers to upload a custom 3D model and select a specific part, configure materials and lead time, and get an instant quote,” said Thompson.


The Thomson Instant 3D Quote Tool provides the benefits of real-time pricing and lead time adjustment as users configure material, quantity and priority.

The instant quote tool is currently available for Thomson 60 Case shafting, extending to applications requiring hardened shafts or pins, with other products in the works, including ball screws and lead screws.

For more information on the Thomson instant quote tool, please visit: https://www.thomsonlinear.com/en/design-tools/instant-3d-quote-tool.

About Thomson

With more than 70 years of motion control innovation and quality, Thomson Industries is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case® Linear Shafting, Ball Screws, Lead Screws, Screw Jacks, Linear Actuators, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of linear motion control solutions serving global commercial, and aerospace and defense markets. Thomson has facilities in North America, Europe and Asia with more than 2000 distributor locations around the world.

Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

 

 

back to top