Skip to content Skip to navigation

05/02/2013 | Learn How to Build Simpler Mobile Off-Highway Machines that are Safer, Cleaner and Cost Less to Operate

WOOD DALE, IL – Thomson introduces www.thomsonlinear.com/moh – a new micro-site that provides substantive educational information detailing how electric linear actuators provide superior performance and significantly simplified operation at a lower cost of operation compared with conventional hydraulic options in mobile off highway (MOH) applications such as construction, road maintenance, farming, forestry, turf and railway vehicles. The site details throttle control, quick attach, hood lift, spool valve control and broom control applications where electric linear actuators can deliver some of the most significant benefits. Visitors will also find ready access to detailed information on all relevant Thomson electric linear actuator products.

“This dedicated site is a resource for OEM engineers to learn more about how to leverage the benefits of superior performing, lower profile and more durable electric linear actuators to build a differentiated mobile off highway machine that will improve their and their customer’s bottom line,” says Rob Gallagher, Marketing Communications Manager for Thomson. “Electric linear actuators eliminate many of the safety risks inherent in hydraulic systems, as well as the fluids and cables required of those systems. Electric actuators offer fewer parts to maintain or replace, higher life cycles and more efficient use of power at all times. They also provide superior heat, vibration and moisture resistance, with better interfacing, speed and feedback options, to further optimize performance.”

http://www.thomsonlinear.com/moh is currently available in English, Chinese and German.

About Thomson

With more than 60 years of motion control innovation and quality, Thomson is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case™ Shafting, ground and rolled Ball Screws, Linear Actuators, Gearheads, Clutches, Brakes, Linear Systems, and related accessories.  Thomson invented the Linear Ball Bushing Bearing in 1945, and has set the standard ever since with an unsurpassed set of mechanical motion control solutions serving global commercial and aerospace & defense markets.  Thomson Industries, Inc. has facilities in North America, Europe and Asia with over 2000 distributor locations around the world.

Thomson, 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); thomson@thomsonlinear.com; www.thomsonlinear.com.

back to top