Skip to content Skip to navigation
Press Release Hero Image

Thomson Supports Elara Aerospace in Record-Seeking Rocket Launch Mission

09.06.2026, Kristianstad, Sweden – Regal Rexnord linear motion solutions brand, Thomson, is supporting Elara Aerospace, an academically led initiative founded at the Technical University of Munich (TUM), with precision linear motion technology for its liquid-fuelled Methalox rocket. The Elara team is seeking to become the first student group worldwide to develop a liquid-propelled rocket capable of exceeding 100 kilometers in altitude while being fully reusable and have space for up to 100 kg of scientific experiments. As part of a joint partnership with sister brands Boston Gear and Kollmorgen, Thomson is providing key actuation components that will support active engine positioning and critical flight control functions. 

The system will use two Thomson PC Series precision linear actuators integrated with Kollmorgen AKM13D servo motors and dual-axis drive systems, along with Boston Gear Micron NemaTRUE™ planetary gearheads. Together, the components form a coordinated motion solution tailored to the application’s performance requirements. 

In the Elara rocket, the actuators will support engine gimbaling, enabling controlled movement within a narrow ±5 degree operating range. The PC Series actuators were selected for their compact design, ball screw-based construction and ability to deliver accurate, repeatable motion in space-constrained applications. 

“Rocket control applications leave very little room for uncertainty. Every commanded movement must be predictable, measurable and easy to verify,” said Anders Karlsson, Business Development Manager for Regal Rexnord’s Linear Motion Division. “For us, the value of this partnership is not only in supplying components but in helping Elara build confidence in the actuation approach before the system moves into flight use. Working closely with the team helped us ensure the motion package fits cleanly within the overall engine control architecture.” 

The actuators were supplied as individual components, giving the Elara Aerospace team flexibility in system design and testing. The motion system is currently being validated on development platforms for use in the rocket’s engine control system. 

“For an academically led team working on active engine control, it was important for us to use components that were not only technically capable but also practical to work with,” said Tom Luca Reinhardt, Founder and CEO of Elara Aerospace. “Thomson’s guidance gave us a clear path for the thrust vector control design without adding unnecessary complexity.” 

For more information on Thomson PC Series precision linear actuators, visit https://www.thomsonlinear.com/en/products/precision-linear-actuators/pc-series or contact customer support at 540-633-3549 or thomson@regalrexnord.com. 

To keep up with the Elara Aerospace team and their mission, visit https://www.elara-aerospace.com/ and follow them on LinkedIn and Instagram. 

About Thomson and the Linear Motion Division Brands of Regal Rexnord

Regal Rexnord’s linear motion brands – Thomson, Nook, and Delevan – have nearly 80 years of achievement in motion control innovation and are the premier producers of Linear Actuators, Linear Ball Bushing® Bearings, Profile Rail Linear Guides, 60 Case® LinearRace® Shafting, Ground and Rolled Ball Screws, Lead and Acme Screws, Screw Jacks, Linear Units, Robot Transfer Units, resolvers, magnetics, and related accessories. Ever since inventing the Linear Ball Bushing Bearing in 1945, our brands have set the standard with an unsurpassed set of linear motion control solutions serving global material handling, industrial automation, medical and health, food and beverage processing, aerospace and defense, mobile off-highway, and many other markets through engineering, manufacturing and sales facilities in North America, Europe and Asia.  

For more information on Regal Rexnord brand, Thomson,., 2400 Curtiss Street, Downers Grove, IL 60515; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@regalrexnord.com; www.thomsonlinear.com

 About Regal Rexnord

Regal Rexnord’s 30,000 associates around the world help create a better tomorrow by providing sustainable solutions that power, transmit and control motion. The Company’s electric motors and air moving subsystems provide the power to create motion. A portfolio of highly engineered power transmission components and subsystems efficiently transmits motion to power industrial applications. The Company’s automation offering, comprised of controllers, drives, precision motors, and actuators, and linear systems, controls motion in applications ranging from factory automation to precision tools used in surgical applications. 

The Company’s end markets benefit from meaningful secular demand tailwinds, and include factory automation, food & beverage, aerospace, medical, data center, warehouse, alternative energy, residential and commercial buildings, general industrial, construction, metals and mining, and agriculture. 

Regal Rexnord is comprised of three operating segments: Industrial Powertrain Solutions, Power Efficiency Solutions, and Automation & Motion Control. Regal Rexnord is headquartered in Milwaukee, Wisconsin and has manufacturing, sales and service facilities worldwide. For more information, including a copy of our Sustainability Report, visit www.regalrexnord.com.

Back to press releases
back to top