Skip to content Skip to navigation
Press Release Hero Image

Thomson introduces enhanced configurator for miniature precision lead screws

Kristianstad, Sweden – Thomson Industries, Inc., a leading manufacturer of linear motion control solutions, has announced a significant upgrade to its online lead screw selector tool with enhanced configuration capabilities for its miniature models. Available in diameters of 2, 3 and 4 mm, Thomson miniature lead screws are engineered for applications that demand compact, precise motion – catering specifically to the medical, robotics and automation markets.

The upgraded selector tool introduces a dynamic modal that helps users tailor machining and end support options effortlessly. Users can now configure support ends with standard journal options and select from an array of drive-end configurations, including integrated motor couplers for rapid prototyping and oversized journals compatible with standard market bearings. These features enable users to design custom solutions directly through the Thomson website, streamlining the process from selection to checkout.

“Our goal was to make the configuration process for our miniature lead screws as accessible and efficient as possible, reducing the need for direct engineering support and putting powerful customisation tools at our customers’ fingertips,” Ojesh Singh, product manager, Thomson Industries–EMEA region. “This update reflects our commitment to supporting the prototype cycle, particularly for industries where rapid innovation is key.”

Typical use cases for Thomson miniature lead screws include handheld medical devices such as syringe pumps and grippers, as well as robotics and small-scale automation systems. With an extensive array of configuration options, Thomson addresses diverse application needs while maintaining high standards of performance and reliability. Additionally, Thomson plans to expand similar configurability features to other product lines in the future, reinforcing its dedication to innovation and customer-centric solutions.

For more information on Thomson’s miniature lead screws and to experience the enhanced configurator, visit www.thomsonlinear.com/ls.

About Thomson Industries, Inc.

With more than 75 years of achievement in motion control innovation and quality, Thomson is the industry’s premier producer of Linear Actuators, Linear Ball Bushing® Bearings, Profile Rail Linear Guides, 60 Case® LinearRace® Shafting, Ground and Rolled Ball Screws, Screw Jacks, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945 and has set the standard ever since with an unsurpassed set of linear motion control solutions serving global aerospace and defense, medical and health, factory automation, food processing, and mobile off-highway markets. Thomson, a brand of U.S.-based Regal Rexnord Corporation, has facilities in North America, Europe and Asia with more than 2000 distributor locations around the world. For more information Thomson Industries, Inc., 2400 Curtiss Street, Downers Grove, IL 60515; 1-540-633-3549; 1- 540-633-0294 (fax); Thomson@regalrexnord.com; www.thomsonlinear.com.

Back to press releases
back to top