Skip to content Skip to navigation

4/8/2015 | You Wanted Them but Didn’t Want to Wait: Thomson Switches its Popular SB Series Brakes Line to Fast Delivery Program

04.08.2015, WOOD DALE, IL – Thomson Industries Inc., a leading manufacturer of mechanical motion solutions, has introduced a new express shipping service for its SB Series power off brakes. The service is provided as standard option and does not require a premium or a fee. It offers customers 24-48 hours shipments on most options in the range, including all 10 available frame sizes.

The express shipping service offers customers the benefits of the SB Series brakes, which are faster, and higher performing than many other servo-brake models, the express program will reduce delivery time for customers. They are designed to last longer and meet safety and regulatory requirements across numerous markets including personal automation. They offer the highest spring set braking torque to size ration in the market, resulting in a compact and light solution that is easier to integrate into machine designs.

SB Series products are further designed to withstand severe environmental conditions. They have a class H insulation system that covers temperatures up to 180 °C and a fully potted coil that resists environmental contaminants such as dust, dirt and humidity. They also come as standard with a zinc plating to protect from rusting. The precise engineering and robust nature of the SB brakes ultimately means they are designed to give longer life and work in almost any environment.

The principal behind the design of the SB Series brakes is straightforward: They are designed to work, whatever happens; They are resistant to high shock loads, work well in temperatures up to 180 degrees C, and are resist to dirty, dusty conditions. The SB Series will carry on giving exceptional performance, reliability and assured safety.

Custom variations of the SB Series brakes, including adaption for use in rigorous outdoor environments, are available. Contact Thomson Customer Support for more information on available options.

Thomson has a continuing program of research and development to help ensure its customers can meet the modern challenges they face in competitive market places. The SB Series brakes are just one example of the Thomson’s expert engineering and market-leading solutions and their new rapid delivery part of its commitment to customer support excellence.

For more information about the SB Series please visit:
http://www.thomsonlinear.com/website/com/eng/products/clutches_and_brakes/friction/standard_power_off.php

To learn more about the SB Series Brake express program please visit:
http://www.thomsonlinear.com/downloads/clutches_brakes/Clutch_Brake_Express_SB_Series_bren.pdf

About Thomson

With more than 70 years of motion control innovation and quality, Thomson is the industry’s premier producer of Linear Ball Bushing® Bearings and Profile Rail Bearings, 60 Case® Shafting, ground and rolled Ball Screws, Linear Actuators, Gearheads, Clutches, Brakes, Linear Systems, and related accessories. Thomson invented the Linear Ball Bushing Bearing in 1945, and has set the standard ever since with an unsurpassed set of mechanical motion control solutions serving global commercial and aerospace & defense markets. Thomson Industries, Inc. has facilities in North America, Europe and Asia with over 2000 distributor locations around the world.

Thomson Industries, Inc., 1500 Mittel Boulevard, Wood Dale, IL 60191-1073; 1-540-633-3549; 1-540-633-0294 (fax); Thomson@thomsonlinear.com; www.thomsonlinear.com.

Click to Enlarge Images:

back to top