Skip to content Skip to navigation

What is the difference between pitch and lead when referring to a screw?

Pitch is the distance between screw grooves and is commonly used with inch sized products and specified as threads per inch. Lead is the linear travel the nut makes per one screw revolution and is how ball screws are typically specified. The pitch and lead are equal with single start screws.  For multiple start screws the lead is the pitch divided by the number of starts.

http://www.thomsonlinear.com/website/com/eng/training/difference_between_screw_pitch_and_lead.php

back to top