Thomson currently has two account systems - one for the website and CAD model downloads, and one for e-commerce. We understand that two logins is an inconvenience and are working to consolidate our systems into one login process. Until we’re able to consolidate the two logins, please follow these guidelines:
Customer Service Chat (ONLINE) Customer Service Chat (OFFLINE)
Thomson RoundRail shafting is manufactured to the highest quality standards in an ISO 9001:2015 registered facility to provide industry leading surface finish, roundness, straightness and cylindricity. Thomson offers the widest selection of linear shafting in the industry to ensure optimal performance, minimal maintenance and long life.
Need shafting ASAP for your design project? Watch to learn how Thomson delivers quickly across North America.
Click here to optimize your design with a custom shafting solution.
With more than 70 years’ experience as one of few suppliers that produces its own precision bearing shafts, Thomson provides best-in-class case hardness and depth, surface finish, roundness, straightness and cylindricity. And when used with Thomson Linear Ball Bushing® Bearings, travel life and load capacity are significantly increased compared to conventional models.
When your linear motion projects require shafting that doesn’t fit within our standard offering, Thomson skilled machinists can perform a wide variety of special machining operations on the ends or along the length of the 60 Case® shaft to provide the exact part needed for your application. Examples of our customization capabilities include drilling and/or tapping, special tolerances, milling, turning, extended lengths, special coatings/finishes and many more.
Thomson provides extensive online resources to help you no matter where you may be in the roundrail shafting purchase decision process:
Thomson 60 Case Linear Race shafting has been popular for decades for its consistent reliability and performance. To help customers get this high-quality, lab-tested product into their hands as quickly as possible for their time-sensitive design projects, Thomson goes to great lengths.
With the special machining add-on to the Thomson online shafting selector tool, the burden of creating 2D drawings is relieved, and the amount of time needed to specify the machined shaft is dramatically reduced.
Watch this comprehensive demo and see how this feature offers the most commonly used machining options, which are automatically converted to manufacturable 2D drawings for download as printable PDFs or sharable links.
Try the online shafting selector tool and special machining add-on at: https://www.thomsonlinear.com/en/products/shafting
For any cases in which your machining configurations don't fall within the scope of our tool's options, Thomson application engineers are always ready to provide fast help.
Maximize the performance and life of your linear motion systems by knowledgeably choosing the optimal shafting. All it takes is becoming familiar with a few key considerations.
Don't wait so long for a customized shafting quote. Simply upload your 3D model and get instant pricing and lead time on custom 60 Case LinearRace shafting.
Properly mounting round shafting is required for it to be used as a linear guide. Watch this video to learn about the most common shaft mounting methods.
What is the difference between round rail and square rail? How do you know which one is more appropriate for a given application? How do you size them? Learn the basics of linear guide technology and how to size them for your next application. Plus - get a guided tour through the new online Linear Guide Component Tool.
In this webinar, you will learn: Linear Bearing Types, Typical Applications, Design Considerations, Application Requirements, Optional Features, and Design Calculations.
Advancements in load capacity, life and ease of manufacture allowed an ever-widening range of applications to benefit from nearly friction free linear guidance. Since the introduction of the square, or profile rail, linear guide in the 1970s, the design engineer has been faced with the pivotal question: round or square?
Learn MoreHow to choose between the main types of linear technologies, and how to design automation systems that deliver optimal performance using design requirements, rather than cost, as the primary consideration in selecting linear components.
Learn MoreSpecifying the right bearing for a given application is necessary to save time and excessive costs. Understanding the tradeoffs of each bearing type is important to accurately size and select the right bearing for your application. This article will provide an overview of the major types of linear bearings and guides, explain how to specify them for specific applications and describe how to trouble-shoot common application problems.
Learn MoreUltra Light Aluminum LinearRace Shafting | 976 KB |
60 Case Shafting | |||
60 Case LinearRace Shafting (Inch) | — | — | |
60 Case LinearRace Shafting Assemblies (Inch & Metric) | — | — | |
60 Case LinearRace Shafting Rails (Inch & Metric) | — | — | |
60 Case LinearRace Quick Shafting - QS (Metric) | — | — | |
60 Case LinearRace Quick Shafting - QS (Inch) | — | — | |
60 Case Shafting Support Blocks | |||
Shafting End Support Blocks - ASB (Inch, Low Profile, Aluminum) | — | — | |
Shafting End Support Blocks - ASBM (Metric, Low Profile, Aluminum | — | — | |
T-Case Shafting | |||
T-Case | — | — |
To provide better service to you on our websites, we and our service providers use cookies to collect your personal data when you browse. For information about our use of cookies and how to decline them or turn them off please read our cookie policy [available here].